This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

仿真器XDS560连接目标板C6713报错,好久也没弄好,请各位专家指点迷津~



XDS560连接目标板C6713总是报错如下:

Error connecting to the target:

Error 0x80000200/-233

Fatal Error during: OCS,

This error was generated by TI's USCIF driver.

SC_ERR_PTH_BROKEN <-233>

An attempt to scan the JTAG scan-path has failed.

The target's JTAG scan-path appears to be broken

with a stuck-at-ones or stuck-at-zero fault.

Sequence ID: 0

Error Code: -233

Error Class: 0x80000200

Board Name: C671x XDS560 Emulator

Cpu Name: TMS320C6710_0

Abort: Close Code Composer Studio.

Retry: Try to connect to the target again.

Cancel: Remain disconnected from the target

Diagnostic: Run diagnostic utility.