This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Windows Embedded CE6.0 BSP Support BeagleBoneBlack and Capes Now



Hi, All


We now support Windows Embedded CE 6.0 OS running on BeagleBone and BeagleBoneBlack Boards, with BeagleBoneBlack Capes together.

Our BSP Features are as following:

  • High Speed eMMC Support
  • SDHC Micro SDCard Support Upto 32G
  • 512MB DDR3
  • Persistend Registry Support
  • HDMI Display Support (1280x720)
  • LCD Display Support (800x480,1024x600,800x600,480x272 and so on)
  • RS232/RS485 Support
  • GPIO Button Support
  • Backlight Support
  • USB OTG & HOST Support
  • SPI Bus and I2C Bus Support
  • Resistive and Capactive TouchScreen Support
  • AIC3106 Audio Support  
  • CPGMAC Ethernet Support
  • NANDFlash Support with Firmware into NAND and Bootlogo update dynamically
  • External I2C RTC Chip Support
  • WL1271 Support (IF NEED)
  • NLED Support
  • Auto-Run Programs

 

For anyone who are interested, pls access the web:

http://bbblackwince6bsp.codeplex.com


For any other information, pls contact through email:  dev2013@live.cn

Thanks & Best Regards,

Stephen Zhang