最近做了两块DM6467视频板,第一块功能完好,第二块用下载UBL和UBOOT出现问题,ARM始终连不上,报错:
Warning:
0x40000220/-2062 @ marker 13500
Warning during: Execution, OCS,
Cannot halt the processor
打了下24M和33M晶振电压,24M为1.2V,33M基本为0V,不知道是不是DM6467没焊接好还是晶振坏了,求高手帮助啊
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
最近做了两块DM6467视频板,第一块功能完好,第二块用下载UBL和UBOOT出现问题,ARM始终连不上,报错:
Warning:
0x40000220/-2062 @ marker 13500
Warning during: Execution, OCS,
Cannot halt the processor
打了下24M和33M晶振电压,24M为1.2V,33M基本为0V,不知道是不是DM6467没焊接好还是晶振坏了,求高手帮助啊
是的,晶振也换过了,电压依然这样,测了dm6467的供电电压都是对的,ccs就是无法识别ARM这端
你好,
DM6467的DEV_MXO是否有输出?这是看晶体是否起震。
可以把DM6467配置为uart0启动,看串口是否有bootme出来。
我怀疑是芯片没有正常工作,这样CCS是连不上DM6467的。
DEV_MXO几乎没有输出,串口也没有bootme。估计是6467没有正常工作,我测过6467电源都是好的,BGA焊接也检测过没有虚焊,难道6467坏了?