This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于调用C67x FastRTS Library的问题??



我从TI官网上下载了C67x FastRTS Library:c67xmathlib_2_01_00_00_Windows_Setup.exe

默认安装在C:\c67xmathlib_2_01_00_00 路径下,

然后在Link.cmd文件中加入:

-l C:\c67xmathlib_2_01_00_00\lib\c674xfastMath.lib

在C语言源文件中加入:

#include "C:\c67xmathlib_2_01_00_00\inc\c67fastMath.h"

编译时出现30个error:

"C:\c67xmathlib_2_01_00_00\inc\../src/sp/atan2sp/atan2sp.h", line 15: error: expected a ")"

"C:\c67xmathlib_2_01_00_00\inc\../src/sp/atansp/atansp.h", line 15: error: expected a ")"

"C:\c67xmathlib_2_01_00_00\inc\../src/sp/cossp/cossp.h", line 15: error: expected a ")"

"C:\c67xmathlib_2_01_00_00\inc\../src/sp/divsp/divsp.h", line 15: error: expected a ")"

…………

如果将FastRTS安装目录下的.lib文件拷到CCS4.2默认安装目录:

C:\Program Files\Texas Instruments\ccsv4\tools\compiler\c6000\lib  下,

FastRTS安装目录下的.h文件拷贝到:

C:\Program Files\Texas Instruments\ccsv4\tools\compiler\c6000\include  下,

然后在Link.cmd文件中加入:

-l c674xfastMath.lib

在C语言源文件中加入:

#include <c67fastMath.h>

编译时出现一个error:C:/Program Files/Texas Instruments/ccsv4/tools/compiler/c6000/include/c67fastMath.h",

line 17: fatal error: could not open source file "../src/sp/atan2sp/atan2sp.h"

1 fatal error detected in the compilation of "../main.c".

Compilation terminated.

我本意是想调用里面的一些函数做运算,提升速度,但这是什么情况???

要怎样做才能顺利调用这这些函数??