您好:
我使用的CCS版本是release版本:CCS5.1.0.09000,MCSDK版本是最新版本:bios_mcsdk_02_00_05_17,ccs安装在C:\ti路径,MCDSK安装在C:\Program Files\Texas Instruments路径.
将工程添加到CCS中后,添加C:\Program Files\Texas Instruments\pdk_C6678_1_0_0_17\packages\ti\drv\macros.ini,这个用来设置pdk工程的路径,编译后报错如下:
1.Buildfile generation error occurred..
RTSC product-type 'com.ti.biosmcsdk.pdk.C6678L' is not recognized. Please install at least one product of this type.
警告:
1.Build variable 'TI_PDK_C6678_INSTALL_DIR' cannot be resolved.
2.Invalid project path: Include path not found (\packages).
3.RTSC product 'Inter-processor Communication' v1.24.0.16 (or equivalent) is not currently installed. A compatible version 1.23.5.40 has been used. Please install a product of equivalent version, or enable one of the supported versions of this product.
4.This project was created using a version of compiler that is not currently installed: 7.2.4 [C6000]. Another version of the compiler will be used during build: 7.3.1. Please install the compiler of the required version, or migrate the project to one of the available compiler versions.
请各位TI工程师帮忙解决下,多谢!