Version: 5.2.1.00018
合众达:xds510plus , 开发板 LCDK, gel 文件为:..\..\emulation\boards\lcdkomapl138\gel\OMAP-L138_LCDK.gel ARM 端和DSP端都选上了gel 文件。
问题 1 :CCS连ARM端的时候,出现下面错误:
ARM9_0: Output: Memory Map Setup Complete.
ARM9_0: Output: ---------------------------------------------
ARM9_0: GEL: Error while executing OnTargetConnect(): Attempted to read unmapped virtual memory at 0x01C10800 at (*((unsigned int *) ((0x01C10000+0x800)+(4*LPSC_num)))&0x1F) [OMAP-L138_LCDK.gel:868] at PSC0_LPSC_enable(0, 0) [OMAP-L138_LCDK.gel:509] at PSC_All_On() [OMAP-L138_LCDK.gel:244] at OnTargetConnect() .
ARM9_0: Trouble Writing Memory Block at 0x80005908 on Page 0 of Length 0x1b4
ARM9_0: GEL: File: D:\workspace_v5_2\test-arm\Debug\test-arm.out: Load failed.
ARM9_0: Unable to terminate memory download: NULL buffer pointer at 0x320
问题2: test connection xxx.ccxml时出现如下错误:
This utility has selected a 100- or 510-class product.
This utility will load the adapter 'seedjca8990isa.dll'.
An error occurred while soft opening the controller.
-----[An error has occurred and this utility has aborted]--------------------
This error is not generated by TI's USCIF driver or utilities.
The USCIF driver and utilities use the range from -2 down to -999
请TI的专家给予帮助解决,谢谢。