This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请问dm385支持超低码流吗?



dm385能否支持,720P:1-2M,1080P:2-4M。

  • 我们也遇到了同样的需求,不知道DM385的Codec能不能做到这一点。

    我们目前的平台是DM368,客户的期望是720P@25fps的码流降到512k-1M。

    以目前368的能力,似乎达不到这一点。因此我们目前采取的策略是,在低带宽的环境下,打开KNF+TNF,这样可以大大降低带宽的要求,但是这样却大大影响了画质。所以说,这种策略还是有很大的限制。

    不知道,TI的专家们有什么建议,能否在目前DM368的基础上,在H.264的Encode的参数配置方面做点工作?

  • 你好,

    一般来说DM385可以支持你说的码流。但实际应用上,还是要看你使用的是CBR,还是VBR,以及QP范围的设置。如果参数配置不合理,会导致码率和预期不一致。

    对于DM36x,如果你选择CVR,可实现低码率,但是会丢帧。低码率下建议使用rcalg=5.