This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6657: 编译器会如何解释void interrupt GPIO_ISR_test(void)

Part Number: TMS320C6657

请问编译器在解释

void interrupt GPIO_ISR_test(void)

和

void GPIO_ISR_test(void)

时会有什么区别呢?

最近我在调试同事遗留下来的6657工程,工程中使用了第三方的库文件“C6657_Driver_Lib.lib”,该库文件中,注册中断函数的函数声明如下:

Bool  C6657_CoreInt_Set (Uint16 EventId,Uint8 VectId,void  interruptISR(),void* Param);

由于只是提供了库文件,所以我不知道这个注册中断函数的定义

调试过程中发现,如果中断函数定义为void interrupt GPIO_ISR_test(void),那么程序执行后会很快跑飞;

如果中断函数定义为void GPIO_ISR_test(void),则执行是正常的。

当中断函数定义为void interrupt GPIO_ISR_test(void)时,

C6657_CoreInt_Set (89,15,GPIO_ISR_test,NULL);通过中断注册函数中的GPIO_ISR_test无法定位到中断函数的定义,但是编译并没有报错。

 

所以我想,编译器对void interrupt GPIO_ISR_test(void)的编译结果是不是和void GPIO_ISR_test(void)不一样,想请教一下