This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM4376: boot启动问题

Part Number: AM4376


我们使用AM4376处理器设计的核心板,部分板卡无法从boot启动,具体情况如下:
   1、处理器型号是:AM4376BZDNA100,时钟24M;
   2、电路设计的启动方式:可以从MMC1、MMC2、NAND启动;
   3、sysboot管脚[18..0]的配置为:000 0100 0010 0000 0100  (后四位可以配置成0110、1100),通过XDS100确认启动配置管脚读取与实际电路一致;
   4、目前的现象是部分板卡可以正常启动,但是部分板卡MMC1、MMC2、NAND三种启动方式都无法启动;
   5、通过XDS100跟踪寄存器,发现无法启动的板卡,对应的mmc、nand等管脚均没有进行配置,采用默认mod7;同时Boot Error Counters也没有进行错误计数,是随机的数值(正常板卡读取的数值是3次、2次或者0次);从现象上来看,感觉是4376的内部boot没有运行;
  6、对比启动正常板卡和异常板卡的CONTROL寄存器,CTRL_CORE_SLDO、CTRL_MPU_SLDO寄存器数值不一致,正常板卡读取的数值为02FD0000,异常板卡读取的数值为001F0000;