This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCIe转接板

Other Parts Discussed in Thread: TMDXEVMPCI

您好,我买了一块TMDXEVMPCI,然后与6678L评估板连接在一起,插在主机板上,但是利用windriver却搜不到该板卡。所以我想咨询一下,是不是还需要进行一些设置?谢谢!

  • 您好,

    可以参考一下这个帖子,下面有说明。有问题可以继续讨论。

    关于TMS320C6678EVM的PCIe接口性能问题

    www.deyisupport.com/.../5114.aspx

  • 您好,谢谢您的回复。

    我按照文件上的步骤依次更新了IBL和IBL的配置,然后根据下面的switch设置为PCIE BOOT模式:

    switch     pin1    2      3      4

    SW3:       off     on     on     off

    SW4:       on      on     on     on

    SW5:       on      on     on     off

    SW6:       off     on     on     on

    SW9:       on

    但是在windriver中还是找不到板卡,请问是不是还需要什么配置?或者可能会有什么错误?谢谢!!

  • 您好,

    请确认使用MCSDK_2_05_07以上版本中的IBL。

  • 您好,谢谢您的及时回复。

      我起初用的版本低了,现在我又用MCSDK_02_00_05_17版本配置了一遍。但是,在设备管理器中还是没找到新的设备。IBL和IBL的配置都显示结果成功了,switch也是按照文档操作的,为什么还是找不到板卡呢?是不是还有其他被我忽略的操作啊?

      谢谢您了!