This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于OMAP-L138的boot问题

Other Parts Discussed in Thread: OMAP-L138

您好!在使用OMAP-L138芯片遇到以下问题,特在此咨询一下,谢谢!

现象:外部配置bootmode是NOR FLASH,我们试图通过Norflash启动,但当OMAP-L138芯片上电后,OMAP-L138芯片的管脚的BOOT[7:0]无法读取外部配置的0000 0010,通过仿真器读取的Bootcfg的value:0000 0000。

上电时序:OMAP-L138芯片1.2V先上电,延时100ms后1.8V起来,延时100ms后3.3V起来,最后延时400Ms释放OMAP-L138的reset信号(说明:reset信号是由单片机GPIO管脚发出低电平信号,然后该GPIO管脚变为高阻抗,reset信号状态由OMAP-L138芯片内部弱上拉决定)。请问这样的上电时序设计是否有问题?

    另外特此请教一下,boot信号和reset信号二者上电后的拓扑关系是否可以提供一下吗?除此之外,是否还有其他因素导致出现这种现象的?

备注:1. reset信号的测试波形请参看附件1,我们板子的reset信号(上升时间为500us),对比合众达开发板的reset信号(上升时间为15us),这样是否有问题?

            2. 原理图设计部分请参看附件2。