This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8168 U-Boot烧写问题



在DM8168 DVR-UD1板子上 按照文档《DM8168_DVR_RDK_Install_Guide.pdf》中的说明,编译并烧写U-Boot后启动不起来, 1. 按1.4.4节,编译U-Boot和Kernel; 2. 按1.4.3.3.1节,配置TFTP服务器,烧写编译好的kernel,OK,能够正常启动Linux; 3. 按1.4.3.2.2节,先从NAND Flash启动U-Boot,然后利用TFTP烧写编译的U-Boot到NAND Flash; 烧写显示成功;但是重启后就起不来了,串口没显示; 4. 想从SD卡启动然后恢复U-Boot,按1.4.3.2.1节操作,还是起不来,串口没有打印(应该是启动失败,serial没有初始化); 5. 按1.4.3.2.3节,从EMAC启动,失败。 想问下: 如何从SD卡启动,是否还有其他要求,比如所SD卡格式方式,容量等? ps:怕编译的版本有问题,SD卡里用的是包里自带的版本;我们的SD卡用的是索尼4G卡,class4;格式是FAT32。 关于从EMAC启动,前提也是要先启动u-boot,再用u-boot命令配置环境,这个u-boot启动的是哪里的? 附件包含pdf文档、MLO和u-boot.bin是包里自带的SD卡启动文件、u-boot_dvr.noxip.bin和uImage_dvr是编译的U-Boot和Linux kernel。 谢谢!
u-boot.rar