This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

我遇到关于OMAP3530的问题

Other Parts Discussed in Thread: TPS65930

1、电源管理芯片TPS65930

板子上电启动后,没有电源输出,用手碰一下32K晶振,电源VIO、VDD1、VDD2才会有输出。有时候是等待30秒左右,电源会有输出。

32K的晶振起振正常,用示波器看波形很好,但从TPS65930输出的时候不是很正常,有31.5K左右。有一块板子同样的芯片,输出只有10K左右。

2、电源输出正常后,串口3能打印出ROM CODE,但是不能从SD卡启动,VMMC有3V,SYSBOOT0~SYSBOO5设置为111100,不知道是什么原因。

请教各位高手帮忙解答疑问。谢谢!