This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DMVA3/4相关问题



你好!

我们目前在做一个视频监控的产品,想采用DMVA3来设计。当前的技术资料不全,请问几个问题。

1、DMVA3支持BT1120(16位)标准视频接口,请问是否支持内同步和外同步两种模式?

2、DMVA3参考设计时采用两颗1Gb的DDRIII颗粒,可否采用1颗2Gb的DDRIII颗粒来设计?若视频处理为1080P/60FPS,2Gb的内存是否够用?

3、DMVA3有一个视觉协处理器,该处理器可以实现那些智能分析功能?

4、那些途径可以获得更全面的技术资料?

 

  • 你好,

    1.可以支持。下面的信息在DMVA的数据手册里面可以找到。

    • Parallel Camera (CAM) interface features:
    – Input format
    • Bayer pattern Raw (up to 16bit) or YCbCr 422 (8bit or 16bit) data.
    • ITU-R BT.656/1120 standard format
    – Generates HD/VD timing signals and field ID to an external timing generator, or can synchronize to
    the external timing generator.

    2. DMVA的DDR接口是32位的,如果你提到的2Gb DDR3芯片也是32位的,就可以。1080p60的应用是指的纯编码么?是否使用2Gb DDR足够,是取决于你的应用程序有多复杂。

    3. 在DMVA的参考设计里面有介绍文档。DVMA的性能也请参考参考设计相关文档。

  • 非常感谢你的回答。

    1、Camera Interface CAM[D0]-CAM[D15]和BT1120的Y0-Y7\CbCr0-CbCr7如何对应?另外VideoInput 0(Digital)与Camera Interface 都支持BT1120输入,设计时如何选择视频输入通道呢?

    2、我们目前的参考文档不全,只有一份简单的datasheet,可否在这介绍一下DMVA3的智能分析功能,另外和DM8127的智能分析功能有和差异?