This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于OMAP_L138的SDK问题?



最近在用omap_l138做驱动部分的移植工作,使用CCS5.4的IDE在windows XP系统上进行开发,TI提供的官网上有MCSDK和C6SDK这两个SDK,说明文档里面说这两个SDK都支持OMAP_L138的开发,所以将这两个SDK都安装了,代码还是看C6SDK为主,在C6SDK的安装目录下面有startware这个支持包,里面有uartecho的例程,其中在中断配置的时候有进行宏定义的预编译,可以选择中断挂接到DSP的内核或者ARM的内核,但是其中挂接到DSP的内核的函数可以在intterupt.c里面找到,但是挂接到ARM中断的相关函数,比如:IntAINTCInit();和IntMasterIRQEnable();函数在CCS的目录下没有找到,在C6SDK的目录下也没有找到,在MCSDK的目录下面也没有找到,三个问题请大家知道的话请告诉我:

1.  开发OMAP_L138使用C6SDK还是MCSDK?

2. ARM内核相关的IntAINTCInit();和IntMasterIRQEnable();这些函数在哪里?是不是一定要去Linux里面自己移植过来还是TI官方也提供ARM的内核的库?

3. 为什么MCSDK的安装目录下面的例程只有MCASP和MCBSP这两个例程,没有像C6SDK下面的startware一样有每个外设的示例,还有每个外设和EDMA3一起使用的示例?

  • 你好!

    1. 都可以

    2.按照你帖子的描述,我理解你是在OMAPL138进行非OS的开发。

    有OMAPL138的单独的starterware可以下载,不用下载完整的SDK包。

    上述两函数在system_config\armv5\OMAPL138\interrupt.c中有定义

     

  • 您好,谢谢你给我的答复,但是还有一个问题不明,请指教,就是我现在用omap_l138进行开发,操作系统用TI的sys/bios,ARM内核和DSP内核都要用这个操作系统,双核还需要通信的,但是不使用GIO,只使用startware,请问是不是只要CCS5和omap_l138 startware就好了?还是需要装MCSDK或者C6SDK之类的SDK嘛?