This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM625: 字符设备驱动的使用:内核无法使用of_get_named_gpio获取,请问当前内核不支持字符设备驱动硬件吗?还是通过什么地方配置支持,还是怎么办

Part Number: AM625


SDK版本08.03.00.19
//驱动编译后能找到节点

leddev.node = of_find_node_by_path("/led6254");
if (leddev.node == NULL){
printk("gpioled node nost find!\r\n");
return -EINVAL;
}
else{
printk("led6254 find !\r\n");
}

//驱动编译后不能通过of_get_named_gpio();函数找打引脚,启动日志显示 -22
leddev.led0 = of_get_named_gpio(leddev.node, "led6254-gpio", 0);
if (leddev.led0 < 0) {
printk("can't get led6254-gpio\r\n");
return -EINVAL;
}

报错如下

[ 0.905759] led driver and device was matched!

[ 0.910570] led6254 find !

[ 0.913447] can't get led6254-gpio

[ 0.917029] imx6ul-led: probe of led6254 failed with error -22

  • 我咨询一下相关工程师再给你回复。

  • 请问是想要获取gpio number吗?

    您是修改的哪个内核驱动程序?

    这个 gpio 的设备树设置是什么?

  • 这是设备树的pinctrl:

    led6254 {
    compatible = "led6254";
    status = "okay";
    pinctrl-names = "default";
    pinctrl-0 = <&usr_led6254_pins_default>;
    led6254-gpio = <&main_gpio1 16 GPIO_ACTIVE_LOW>;
    };

    这是设备树的pinctrl:

    usr_led6254_pins_default: usr-led6254-pins-default{
    pinctrl-single,pins = <
    AM62X_IOPAD(0X1B8,PIN_OUTPUT,7)
    >;
    };

    这个是驱动代码:我想用字符设备方式来驱动gpio

    #include <linux/types.h>
    #include <linux/kernel.h>
    #include <linux/delay.h>
    #include <linux/ide.h>
    #include <linux/init.h>
    #include <linux/module.h>
    #include <linux/errno.h>
    #include <linux/gpio.h>
    #include <linux/cdev.h>
    #include <linux/device.h>
    #include <linux/of_gpio.h>
    #include <linux/semaphore.h>
    #include <linux/timer.h>
    #include <linux/irq.h>
    #include <linux/wait.h>
    #include <linux/poll.h>
    #include <linux/fs.h>
    #include <linux/fcntl.h>
    #include <linux/platform_device.h>
    //#include <asm/mach/map.h>
    #include <asm/uaccess.h>
    #include <asm/io.h>

    #define LEDDEV_CNT 1
    #define LEDDEV_NAME "dtsplatled"
    #define LEDOFF 0
    #define LEDON 1

    struct leddev_dev{
    dev_t devid; /* 设备号 */
    struct cdev cdev; /* cdev */
    struct class *class; /* 类 */
    struct device *device; /* 设备 */
    int major; /* 主设备号 */
    struct device_node *node; /* LED设备节点 */
    int led0; /* LED灯GPIO标号 */
    };

    struct leddev_dev leddev; /* led设备 */

    /*
    * @description : LED打开/关闭
    * @param - sta : LEDON(0) 打开LED,LEDOFF(1) 关闭LED
    * @return : 无
    */
    void led0_switch(u8 sta)
    {
    if (sta == LEDON )
    gpio_set_value(leddev.led0, 0);
    else if (sta == LEDOFF)
    gpio_set_value(leddev.led0, 1);
    }

    static int led_open(struct inode *inode, struct file *filp)
    {
    filp->private_data = &leddev; /* 设置私有数据 */
    return 0;
    }

    static ssize_t led_write(struct file *filp, const char __user *buf, size_t cnt, loff_t *offt)
    {
    int retvalue;
    unsigned char databuf[2];
    unsigned char ledstat;

    retvalue = copy_from_user(databuf, buf, cnt);
    if(retvalue < 0) {

    printk("kernel write failed!\r\n");
    return -EFAULT;
    }

    ledstat = databuf[0];
    if (ledstat == LEDON) {
    led0_switch(LEDON);
    } else if (ledstat == LEDOFF) {
    led0_switch(LEDOFF);
    }
    return 0;
    }

    static struct file_operations led_fops = {
    .owner = THIS_MODULE,
    .open = led_open,
    .write = led_write,
    };

    static int led_probe(struct platform_device *dev)
    {
    printk("led driver and device was matched!\r\n");
    /* 1、设置设备号 */
    if (leddev.major) {
    leddev.devid = MKDEV(leddev.major, 0);
    register_chrdev_region(leddev.devid, LEDDEV_CNT, LEDDEV_NAME);
    } else {
    alloc_chrdev_region(&leddev.devid, 0, LEDDEV_CNT, LEDDEV_NAME);
    leddev.major = MAJOR(leddev.devid);
    }

    /* 2、注册设备 */
    cdev_init(&leddev.cdev, &led_fops);
    cdev_add(&leddev.cdev, leddev.devid, LEDDEV_CNT);

    /* 3、创建类 */
    leddev.class = class_create(THIS_MODULE, LEDDEV_NAME);
    if (IS_ERR(leddev.class)) {
    return PTR_ERR(leddev.class);
    }

    /* 4、创建设备 */
    leddev.device = device_create(leddev.class, NULL, leddev.devid, NULL, LEDDEV_NAME);
    if (IS_ERR(leddev.device)) {
    return PTR_ERR(leddev.device);
    }

    /* 5、初始化IO */

    //驱动编译后能找到节点

    leddev.node = of_find_node_by_path("/led6254");
    if (leddev.node == NULL){
    printk("gpioled node nost find!\r\n");
    return -EINVAL;
    }
    else{
    printk("led6254 find !\r\n");
    }

    //驱动编译后不能通过of_get_named_gpio();函数找打引脚,启动日志显示 -22
    leddev.led0 = of_get_named_gpio(leddev.node, "led6254-gpio", 0);
    if (leddev.led0 < 0) {
    printk("can't get led6254-gpio\r\n");
    return -EINVAL;
    }
    else{
    printk("led6254 get!\r\n");
    }


    gpio_request(leddev.led0, "led0");
    gpio_direction_output(leddev.led0, 1); /* led0 IO设置为输出,默认高电平 */
    return 0;
    }

    /*
    * @description : platform驱动的remove函数,移除platform驱动的时候此函数会执行
    * @param - dev : platform设备
    * @return : 0,成功;其他负值,失败
    */
    static int led_remove(struct platform_device *dev)
    {
    gpio_set_value(leddev.led0, 1); /* 卸载驱动的时候关闭LED */
    gpio_free(leddev.led0); /* 释放IO */

    cdev_del(&leddev.cdev); /* 删除cdev */
    unregister_chrdev_region(leddev.devid, LEDDEV_CNT); /* 注销设备号 */
    device_destroy(leddev.class, leddev.devid);
    class_destroy(leddev.class);
    return 0;
    }

    static const struct of_device_id led_of_match[] = {
    { .compatible = "led6254" },
    { /* Sentinel */ }
    };

    static struct platform_driver led_driver = {
    .driver = {
    .name = "imx6ul-led", /* 驱动名字,用于和设备匹配 */
    .of_match_table = led_of_match, /* 设备树匹配表 */
    },
    .probe = led_probe,
    .remove = led_remove,
    };

    static int __init leddriver_init(void)
    {
    return platform_driver_register(&led_driver);
    }

    /*
    * @description : 驱动模块卸载函数
    * @param : 无
    * @return : 无
    */
    static void __exit leddriver_exit(void)
    {
    platform_driver_unregister(&led_driver);
    }

    module_init(leddriver_init);
    module_exit(leddriver_exit);
    MODULE_LICENSE("GPL");
    MODULE_AUTHOR("lee");

  • 已帮您转给相关专家。

  • 请参考以下回复:

    The kernel already has a led driver

    The GPIO based led driver is drivers/leds/leds-gpio.c.

    For the device tree configuration, you can refer to the "leds" node in k3-am62a7-sk.dts.