各位大牛:
小弟刚买BB-black板子,想在上面学习sys/bios和NDK,请问可以跑SDK中的ethernet_adapt例程吗?如果不能,需要修改什么呢?请给点建议,谢谢了。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
sysbios支持的ice和idk板子,和bbb的区别还比较大,例如说ddr,pinmux等,如果你要自己porting,工作量还是不小的
是啊,我最近一直在看这方面的东西,好多天了感觉进展不大啊。ddr的话,我现在用的是ICEv2的GEL文件,程序可以正常跑说明ddr没啥问题,pinmux这个简单,应该没啥问题。我就感觉按照NDK那个说明书上的NDK结构,NSP部分三层,我只需要修改MDIO(CSL,第三层)那一层的东西就够了,不知道我的理解对不对?最近发现调试PHY这一层确实太难受了,不知道有人把带sysbios的SDK的东西有没有向BBBlack移植过,有经历的也行啊,求给点建议啊!!!Yaoming Qin 说:sysbios支持的ice和idk板子,和bbb的区别还比较大,例如说ddr,pinmux等,如果你要自己porting,工作量还是不小的
你好!虽然ethernetip_adapter的例子可以在CPSW的网口上跑,但是想要移植在BBB确实改动有些大,ICE_v2上的PHY是TLK110,BBB上的是LAN8710,前者用的是RMII2,后者用的是MII1,PINMUX要改,PHY驱动也要改。
建议你购买一块ICE的板子,在上面做调试,相关信息请参考:
您好,Gary Wu :
很感谢你清晰的回答。目前我的情况是网口PHY驱动这块的改动感觉无从下手,不知道能给点建议不?还有就是BBblack的GEL文件,我下的文件上的DDR3配置时钟是266M,如果是400M的话load以后就无法进入主函数,这个情况也没解决。