CCS控制台窗口生成如下,希望老师帮我解决,谢谢!
**** Build of configuration Debug for project MyIndControlPrj ****
"C:\\Program Files\\ti\\ccsv5\\utils\\bin\\gmake" -k all
making ../src/sysbios.aea8fnv ...
gmake[1]: Nothing to be done for `all'.
'Building target: MyIndControlPrj.out'
'Invoking: ARM Linker'
"C:/Program Files/ti/ccsv5/tools/compiler/arm_5.0.1/bin/armcl" -mv7A8 --code_state=32 --abi=eabi -me -g --gcc --define=ECAT_LIMITED_DEMO --diag_warning=225 --display_error_number -z -m"MyIndControlPrj.map" -i"C:/Program Files/ti/ccsv5/tools/compiler/arm_5.0.1/lib" -i"C:/Program Files/ti/ccsv5/tools/compiler/arm_5.0.1/include" --reread_libs --warn_sections --display_error_number --rom_model -o "MyIndControlPrj.out" -l"./configPkg/linker.cmd" "./NeedModule/am335x_indcomm_uart.obj" "./NeedModule/adc.obj" "./UserFunction/TaskUart.obj" "./UserFunction/TaskLed.obj" "./UserFunction/Lcd4X20.obj" "./UserFunction/Key4X4.obj" "./UserFunction/ETHPWM.obj" "./UserFunction/DataPackProc.obj" "./tiescutils.obj" "./main.obj" -l"C:\Program Files\ti\am335x_sysbios_ind_sdk_1.0.0.8\sdk/protocols/ethercat_slave/stack_lib/ecat_slave_stack.lib" -l"C:\Program Files\ti\am335x_sysbios_ind_sdk_1.0.0.8\sdk/starterware/binary/armv7a/cgt_ccs/am335x/evmAM335x/platform/platform.lib" -l"C:\Program Files\ti\am335x_sysbios_ind_sdk_1.0.0.8\sdk/starterware/binary/armv7a/cgt_ccs/am335x/drivers/drivers.lib" -l"C:\Program Files\ti\am335x_sysbios_ind_sdk_1.0.0.8\sdk/starterware/binary/armv7a/cgt_ccs/am335x/system_config/system.lib" -l"C:\Program Files\ti\am335x_sysbios_ind_sdk_1.0.0.8\sdk/platform/am335x/lib/am335x_platform.lib" -l"C:\Program Files\ti\am335x_sysbios_ind_sdk_1.0.0.8\sdk/os_drivers/lib/sys_bios_driver.lib" -l"rtsv7A8_A_le_n_v3_eabi.lib" "../am335x.cmd"
<Linking>
'Finished building target: MyIndControlPrj.out'
' '
C:/Program Files/ti/ccsv5/utils/bin/gmake --no-print-directory post-build
"C:\Program Files\ti\am335x_sysbios_ind_sdk_1.0.0.8\sdk/tools/post_build/post_build.bat" "C:/Program Files/ti/ccsv5" "C:/Program Files/ti/ccsv5/tools/compiler/arm_5.0.1" "C:\AM3359_Project\MyIndControlPrj\Debug" "MyIndControlPrj" "C:\Program Files\ti\am335x_sysbios_ind_sdk_1.0.0.8\sdk\tools\isdk_image\" "1" "0" "0x80000000" "0x80000000"
"COMPILER ARM_5_x"
系统找不到指定的路径。
Binary file does not exist in path
finished
' '
**** Build Finished ****