This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM3730的UBOOT,仿真,相关问题

Other Parts Discussed in Thread: DM3730

刚接触DM3730与UBOOT相关的工作,我是做ARM底层这个方向的工作,刚接触DM3730,对DM3730的x-loader、uboot、有些问题:

1)X-loader是TI公司提供的代码,开源吗?可以自己做二次开发吗??

2)UBOOT的目标文件是用什么软件编译的??文件格式是什么??可以在其源代码基础上做二次开发吗??

3)DM3730内部的ARM和DSP的调试接口分别是什么??共用1个JTAG接口吗??

4)我从哪里可以下载到DM3730使用的x-loader和U-Boot??

 

  • 1. x-loader是开源的,可以进行二次开发

    2.u-boot一般是用交叉编译工具编译得到,为二进制,同样是开源的,可以进行二次开发

    3.如果用CCS环境调试,共用一个jtag接口,当然也可以在linux+filesystem+app的方式进行调试

    4.一般SDK包就包含了整个开发环境,目前dm3730提供了android、linux、wince的SDK包:

    http://www.ti.com/product/dm3730