This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6678的INTC问题



关于pdk_C6678_1_0_0_17\packages\ti\csl\example目录下提供的cpintc的测试用例:

1、打开INTC模块CSL_intcOpen (&intcObj, 63, &vectId , NULL)时事件号为什么是63呢?查看手册,

63对应的中断事件是INTC0_OUT(3+8*n)7 Or INTC1_OUT(3+8*(n-4))7,这里的3+8*n和7分别代表什么意

思啊?

2、测试用例中,通过((CSL_CPINTC_RegsOvly)CSL_CP_INTC_0_REGS)->STATUS_SET_INDEX_REG = 3手动

触发了INTC0系统中断3,产生了INTC0_OUT(Event Number = 63)中断事件输出,而在打开INTC模块时将

中断事件号63与CPU中断向量4对应,因此产生CPU中断4。通过CSL_CPINTC_mapSystemIntrToChannel

(hnd, 3 , 3)将系统中断3映射到通道3,而通道3与主机中断3对应,因此产生了主机中断。这样理解正

确吗?

3、测试用例是通过手动触发产生中断,如果是由外部触发产生的中断呢?比如IPC中断,是否只需使能

NMIs和global中断,通过CSL_intcOpen将中断事件91(IPC_LOCAL)与某个CPU中断向量对应(例如中断向量

4),并使能中断事件91,就可响应中断呢?而无需设置什么系统中断与通道的映射关系,还有使能主机

中断呢?关于CPU中断、系统中断、通道、主机中断之间到底是个什么样的关系呢?感觉理解上有点混乱

4、关于IPC中断的触发,看手册上说只需将IPCGRx寄存器的最低位置1即可,那么寄存器的4-31位关于

SRCSx的设置有什么作用?在设置上有什么要求吗?

5、通过查看手册,CPU只能响应12种中断,好像以往的C6000系列都有默认映射,例如:好像中断14与15

是对应定时器0和1中断,那么C6678默认的中断映射关系是什么呢?