This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM642作视频处理---TFT数字屏视频输出泛蓝



整个系统有两路视频输入,两路TFT数字屏显示以及一路VGA输出。
   经过这几天的调试,已经确定视频模块全部工作正常,只有VP1口的TFT输出出现视频泛蓝的问题,通过示波器的观察,发现VP1D2-VP1D9都有数据输出,但是VP1D12-VP1D19都没有数据输出,但是只有B0-B4和G0-G2有数据,其他都没有(输出是565格式)。
   我的VP2口也接了TFT数字屏和VGA输出,两个视频显示都正常。而我的VP1口是视频输入和TFT数字屏显示输出通过对GPIO的设置进行复用的。
   上述泛蓝情况是在VP0作视频输入,而VP1只做视频输出时出现的问题。
   附件给出了该现象照片以及我的原理图,请各位兄弟姐妹帮帮忙啦~~谢谢啦!

程序是基于DSP/BIOS的