This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

matlab和CCS生成的dat文件格式不一样,matlab怎么读取CCS生成的dat文件?



这是matlab生成的dat文件格式:

这是CCS生成的dat文件:

  • 你好,

       CCS的DAT格式,有特殊的说明,第一行是头信息。如果想在Matlab中导入CCS的DAT文件,需要自己写一个Matlab的函数,跳过第一行,然后将每一行的16进制数读进来,注意前面的0x也是需要跳过的。

    Code Composer Studio data file

    A text file that contains one line of header information and stores the data as one sample per line. The data can be in any of the following formats:

    · Hexadecimal

    · Integer

    · Long

    · Float

    The header information for data files uses the following syntax:

    MagicNumber  Format StartingAddress PageNum Length

    MagicNumber: Fixed at 1651.

    Format: A number from 1 to 4, indicating the format of the samples in the file. This number represents a data format: hexadecimal, integer, long, or float. 

    StartingAddress: The starting address of the block that was saved.

    PageNum: The page number the block was taken from.

    Length: The number of samples in the block.

    All header values are assumed to be TI-style hexadecimal values.

  • 您好,我想向您请教一下,如何在CCS里面调用MATLAB生成的mat文件。我看有些论坛上说要先把mat文件转化为dat文件,然后在CCS里调用。但在CCS里面如何调用dat文件呢?希望您能帮忙解答一下,谢谢