This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

dm8168硬件问题

TIDM8168DVR4.0版本的原理图,更改了电源部(分用LTM4644替代了TI的电源方案)和PHY,其他部分未做更改。

问题:

1、用SEED560PLUS连接不上8168,连其他类型的板子没有问题,连接dm8168d的板子出现如附件的问题;

 2ubootDVR4.0自带的UBOOTSD卡启动,启动方式选择SD卡启动,用示波器测SD卡座的1脚(MMC_DAT3),一直是低于1V的状态,串口无任何输出。

 3、测量晶振输出太小,将表笔选择到X10状态下的波形如下图,感觉不太正确。

 4、各个电源的启动顺序如下图所示,均满足:上一种电源启动到80%以上后才开始启动另一种电源。

       3.3V启动好后,启动1V_AVS,时隔2ms左右。 

      1V_AVS启动好后,启动1V_CON,时隔12ms后开始启动。

      1V_CON启动好后,启动1V8,1.8V的启动有少许问题,之前空载时测试没问题。 

      1V8启动好后,启动1V5,也伴随少许问题。

      1V5启动好后,启动0V9

 各个图片见附件。

谢谢各位提供宝贵意见!

dm8168硬件问题.doc