我们自己做的Dm8168开发板,用EZSDK制作的U-boot,在ubuntu12.04下烧写之后,发现ping 不通主机,但是同样的方法,在ubuntu10.04下就可以,请问这是什么原因?
注:1、网线是好的
2、用的是ubuntu12.04 系统 不是虚拟机
3、ubuntu 防火墙已卸载
打印信息为:
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我们自己做的Dm8168开发板,用EZSDK制作的U-boot,在ubuntu12.04下烧写之后,发现ping 不通主机,但是同样的方法,在ubuntu10.04下就可以,请问这是什么原因?
注:1、网线是好的
2、用的是ubuntu12.04 系统 不是虚拟机
3、ubuntu 防火墙已卸载
打印信息为:
你好,
你的描述不是很清楚,请问你想说的是在ubuntu12.04环境编译的uboot,无法ping通主机,而10.04的Ubuntu环境编译的uboot却没有问题,是么?
另外,EZSDK我们只在Ubuntu 10.04上做过验证。
The installation can be forced on a fairly new linux distribution but may not work if you are on a very old linux distribution. Please pass --forcehost as an option to the installer and it should complete the installation on your linux machine. However, we have verified the installation on Ubuntu 10.04 only.
http://processors.wiki.ti.com/index.php/SDK_5.0_Single_Installer_FAQ