怎样才能使我的测试程序下载到我SPI0接口的FLASH芯片上。有没有个详细点的方法。是需要修改CMD文件吗,是怎么修改,下载是用CCS5.2仿真的时候有个load program 就可以吗。我的程序不大,就是一个串口的测试程序。我的电路板是自己画的6747,目前就只接了一个SPI的FLASH,W25X32,没有其他SDRAM的东西。仿真没有问题,就是不知怎么把程序下载到FLASH中,折腾好几天了。初学者
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请问这几天在测试什么呢?
google一下,就可以找到很多资料了。
比如在google中搜索C6747 SPI flash,就很容易找到如下链接
http://processors.wiki.ti.com/index.php/Flashing_the_C6747_EVM
上述有详细的说明如何将你的目标程序固化到SPI flash中。
关于C6747的EVM板,很多资料是公开的,我想你在自己设计C6747的板子时候已经参考了吧
http://support.spectrumdigital.com/boards/evmomapl137/revg/
你好, 最近在做DDR3初始化,遇到几个问题想请教一下.
1. DDR3 的ODT有什么用,SDCFG寄存器里有配置DYN_ODT和DDR_TERM,enable还是disable,enable的话值是多少?主要是不知道有什么用处
2. DDR3_CONFIG_REG_12里的 INVERT_CLKOUT是否使能,这个有什么用处,什么时候使能?
3. ramp window register、ramp control register和leveling control register的值怎么确定,看例子工程,第一步值设置后面两个寄存器的31位,使能和触发leveling。后面又有重新设置这三个寄存器的值。这有什么用处,值怎么确定?
以上问题能否详细说明下,不胜感激,谢谢