This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

对 DM365 IBIS的Model selector感到迷惑



有太多的model在DM365 IBIS模型里面

比如:

BC50B_!PI_LOW_1P8    BC50B_PI_1P8   Model Cell HALF_TERM_SSTL_1P8  |HALF_TERM_SSTL_1P8    etc.

我该怎么选择这些model仿真?

|CELL OPERATING AT TWO VOLTAGES.1.5V/1.8V-DUAL SUPPLY | |SR0 IS SLEW RATE CONTROL BIT WHICH DECIDES THE MODE OF OPERATION |T0 AND T1 ARE TERMINATION BITS WHICH CAUSE NO,HALF,FULL TERMINATION |NO TERMINATION WHEN T0=0 WHEN T1=0 |HALF TERMINATION WHEN T0=1 WHEN T1=0 |FULL TERMINATION WHEN T0=0 WHEN T1=1 |SSTL RECIEVER MODE WHEN CMOSEN = 0 |LVCMOS RECIEVER MODE WHEN CMOSEN = 1能帮我看看这是哪几个寄存器?

 

thank you very much!!!