This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

链接时错误



Error connecting to the target: Error 0x80002240/-121 Fatal Error during: Initialization, OCS, Control, This error was generated by TI's USCIF driver. SC_ERR_CMD_HANDLE <-121> A bad controller handle has been given to a function, either before attempting to open the controller, or after having opened the controller and ignored its error status. Valid controller handles are generated when attempts to open the controller return a clean error status. Sequence ID: 0 Error Code: -121 Error Class: 0x80002240 I/O Port = 240 Board Name: C5509A SEEDXDS510USB Emulator Cpu Name: TMS320C5500_0 Abort: Close Code Composer Studio. Retry: Try to connect to the target again. Cancel: Remain disconnected from the target Diagnostic: Run diagnostic utility.

这个错误怎么办?求帮助啊!谢谢