各位好!
我用的环境是DM8168+DVRRDK_04.00.00.03,现在遇到一个问题:无法从VP口采集到数据。我想加入调试信息,编译HDVPSS的驱动。但是没有找到合适的方法。用HDVPSS_Userguide里面的方法:gmake -s all,不成功。我用的linux是ubuntu.想请教各位,这个是不是需要在ccs中编译才可?请各位不吝赐教!!
非常感谢!!!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
各位好!
我用的环境是DM8168+DVRRDK_04.00.00.03,现在遇到一个问题:无法从VP口采集到数据。我想加入调试信息,编译HDVPSS的驱动。但是没有找到合适的方法。用HDVPSS_Userguide里面的方法:gmake -s all,不成功。我用的linux是ubuntu.想请教各位,这个是不是需要在ccs中编译才可?请各位不吝赐教!!
非常感谢!!!
我的应用场景是:我现在用的采集芯片是TVP7002,输入信源是电脑的VGA信号。支持的分辨率有800*600/1024*768/1280*720/1280*768/1360*768/1440*900.我希望做到有的信源的分辨率切换的时候,程序可以自己识别现在信源的分辨率。但是,在我切换的过程中,经常发生采集不到数据的情况。我打印/mcfw/src_bios6/links_m3vpss/capture/captureLink_drv.c中,函数captureLink_drvProcessData中第九行FVID2_dequeue的输出,发现FVID2_dequeue返回值正确(FVID2_SOK),但是frameList.numFrames为0。所以我希望可以通过加入HDVPSS驱动的调试信息,找到不能采集到数据的原因。
我的应用场景是:我现在用的采集芯片是TVP7002,输入信源是电脑的VGA信号。支持的分辨率有800*600/1024*768/1280*720/1280*768/1360*768/1440*900.我希望做到在信源的分辨率发生变化的时候,程序可以自己识别现在信源的分辨率。但是,在我改变信源分辨率的过程中,经常发生采集不到数据的情况。我打印/mcfw/src_bios6/links_m3vpss/capture/captureLink_drv.c中,函数captureLink_drvProcessData中第九行FVID2_dequeue的输出,发现FVID2_dequeue返回值正确(FVID2_SOK),但是frameList.numFrames为0。所以我希望可以通过加入HDVPSS驱动的调试信息,找到不能采集到数据的原因。