This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6455与DP83865设计RGMII接口千兆网,NDK问题

Other Parts Discussed in Thread: DP83865

您好,我设计了一块6455的板子,PHY选型使用的是DP83865,这个PHY也是TI推荐的一款PHY芯片,EMAC与PHY连接使用的RGMII接口,板子上电后插上网线后电脑上能够显示连接到1G网络。

测试一:我使用NDK2.0.0下面的CLIENT测试程序测试,修改了IP等设置。运行程序打印信息如下:

在PC端PING不通DSP板。检查寄存器发现EMAC地址寄存器值不正确。

测试二:使用\c6455_emac-0.4\c6455_emac_loopback例程测试,运行回环测试程序程序运行到MDIO_initPHY( Handle hMDIO, volatile uint phyAddr )函数中

Do{}while()循环处出不来

 

请教各位我的问题出在哪里,是否是因为PHY芯片选型和开发板不一致造成的NDK对PHY寄存器配置不正确?是否需要修改NDK对PHY的配置,如何更改。

急切希望能够得到大家知道,谢谢!!!

6455网络问题描述.docx