我看到BeagleBone Black用的电源管理芯片是TPS65217C,输出1.5V给DDR3供电,DDR3的芯片是MT41K256M16HA -125:E,但是根据芯片资料,这款芯片的供电电压是1.35V,请问BeagleBone Black电源部分的设计有没有问题,这个板子的使用寿命会不会比较短?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我看到BeagleBone Black用的电源管理芯片是TPS65217C,输出1.5V给DDR3供电,DDR3的芯片是MT41K256M16HA -125:E,但是根据芯片资料,这款芯片的供电电压是1.35V,请问BeagleBone Black电源部分的设计有没有问题,这个板子的使用寿命会不会比较短?
你好,BeagleBone Black上选用的这颗DDR3L芯片是可以兼容DDR3(1.5V)工作电压的。没有任何问题。详细可以参考这颗DDR的芯片资料。
这个地方的确是1.5v,DDR3的芯片文档里提到也可以支持1.5v,所以影响不大:
|
VDD = VDDQ = 1.35V (1.283–1.45V) |
|
Backward compatible to VDD = VDDQ = 1.5V ±0.075V |
|
Supports DDR3L devices to be backward compatible in 1.5V applications |
那我如果选用TPS65910A3A1RSLR给MT41K256M16HA -125:E供电是不是也是没问题的
cheng feng 说:那我如果选用TPS65910A3A1RSLR给MT41K256M16HA -125:E供电是不是也是没问题的
如该ddr的spec描述,其可以兼容 1.5v和1.35v,所以选择的pmic可以提供两者之一即可,tps65910A3A1 可以。