各位TI工程师您们好:
在第一次使用TMS320C6657LS开发板时,遇到了一些问题,急求各位解答,谢谢
1、在插了电源线,网线和XDS200 USB JATG时电脑显示XDS2xx USB Emulator安装失败。所以在电脑设备管理器里面显示一个未知的设备并且是一个感叹号。
2、CCS版本:Version: 5.2.1.00018
TI Emulators 5.0.747.1
bios_mcsdk_02_01_02_06
3、显示的错误:
IcePick_D: Error connecting to the target: (Error -183 @ 0x0) The controller has detected a cable break far-from itself. The user must connect the cable/pod to the target. (Emulation package 5.0.747.0)