另外MS320DM8107 和 385的引脚是兼容的吗
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
DM816x是一种封装。
其他几个芯片你看后缀就知道,一种是CYE封装,一种是AAR封装。
您好,请问DM8148和DM8127的封装是兼容的么?自己查数据手册发现是PCB封装是一致的,原理图封装的话,只有俩个脚不一样(CSI2_DX[4] 和CSI2_DY[4] )。请问是这样的么?
Felix Felix1 说:您好,请问DM8148和DM8127的封装是兼容的么?自己查数据手册发现是PCB封装是一致的,原理图封装的话,只有俩个脚不一样(CSI2_DX[4] 和CSI2_DY[4] )。请问是这样的么?
你好;
pcb封装是一致的,但是引脚不一样,比如DM8127没有VIP1,DM8148有vip 0 和vip1 ,还有dm8148还支持sata ,还有几个相关的引脚的定义也是不一样的;
这个具体需要你核对手册,查看device pin maps ;