This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TI-SDK-am335x-evm-06.00.00.00移植到beaglebone black上DCAN驱动问题

Other Parts Discussed in Thread: TPS65217

我用的是TI-SDK-am335x-evm-06.00.00.00 PSP是linux3.2.0-psp04.06.00.11,为了在BBB上用上CAN总线,对mux33xx.c做了如下修改

修改前

    _AM33XX_MUXENTRY(UART1_CTSN, 0,
        "uart1_ctsn", NULL, " NULL", "i2c2_sda",
        "spi1_cs0", NULL, NULL, "gpio0_12"),
    _AM33XX_MUXENTRY(UART1_RTSN, 0,
        "uart1_rtsn", NULL, " NULL", "i2c2_scl",
        "spi1_cs1", NULL, NULL, "gpio0_13"),
    _AM33XX_MUXENTRY(UART1_RXD, 0,
        "uart1_rxd", "mmc1_sdwp", " NULL", "i2c1_sda",
        NULL, "pr1_uart0_rxd_mux1", NULL, "gpio0_14"),
    _AM33XX_MUXENTRY(UART1_TXD, 0,
        "uart1_txd", "mmc2_sdwp", " NULL", "i2c1_scl",
        NULL, "pr1_uart0_txd_mux1", NULL, "gpio0_15"),

修改后

    _AM33XX_MUXENTRY(UART1_CTSN, 0,
        "uart1_ctsn", NULL, "d_can0_tx", "i2c2_sda",
        "spi1_cs0", NULL, NULL, "gpio0_12"),
    _AM33XX_MUXENTRY(UART1_RTSN, 0,
        "uart1_rtsn", NULL, "d_can0_rx", "i2c2_scl",
        "spi1_cs1", NULL, NULL, "gpio0_13"),
    _AM33XX_MUXENTRY(UART1_RXD, 0,
        "uart1_rxd", "mmc1_sdwp", "d_can1_tx", "i2c1_sda",
        NULL, "pr1_uart0_rxd_mux1", NULL, "gpio0_14"),
    _AM33XX_MUXENTRY(UART1_TXD, 0,
        "uart1_txd", "mmc2_sdwp", "d_can1_rx", "i2c1_scl",
        NULL, "pr1_uart0_txd_mux1", NULL, "gpio0_15"),

对board-am335xevm.c文件进行如下修改:

加入

static struct pinmux_config d_can_bbb0_pin_mux[] = {
    {"uart1_ctsn.d_can0_tx", OMAP_MUX_MODE2 | AM33XX_PULL_ENBL},
    {"uart1_rtsn.d_can0_rx", OMAP_MUX_MODE2 | AM33XX_PIN_INPUT_PULLUP},
    {NULL, 0},
};

static struct pinmux_config d_can_bbb1_pin_mux[] = {
    {"uart1_rxd.d_can1_tx", OMAP_MUX_MODE2 | AM33XX_PULL_ENBL},
    {"uart1_txd.d_can1_rx", OMAP_MUX_MODE2 | AM33XX_PIN_INPUT_PULLUP},
    {NULL, 0},
};

在函数static void d_can_init(int evm_id, int profile)中加入
    case BEAGLE_BONE_BLACK:
        /* Instance Zero */            
        setup_pin_mux(d_can_bbb0_pin_mux);
        am33xx_d_can_init(0);
        /* Instance one */
        setup_pin_mux(d_can_bbb1_pin_mux);
        am33xx_d_can_init(1);
        break;

最后/* Beaglebone Black */
static struct evm_dev_cfg beagleboneblack_dev_cfg[] = {
    {am335x_rtc_init, DEV_ON_BASEBOARD, PROFILE_NONE},
    {clkout2_enable, DEV_ON_BASEBOARD, PROFILE_NONE},
    {tps65217_init,    DEV_ON_BASEBOARD, PROFILE_NONE},
    {mii1_init,    DEV_ON_BASEBOARD, PROFILE_NONE},
    {usb0_init,    DEV_ON_BASEBOARD, PROFILE_NONE},
    {usb1_init,    DEV_ON_BASEBOARD, PROFILE_NONE},
    {mmc1_emmc_init,    DEV_ON_BASEBOARD, PROFILE_NONE},
    {mmc0_init,    DEV_ON_BASEBOARD, PROFILE_NONE},
    {d_can_init,    DEV_ON_BASEBOARD, PROFILE_NONE},// 加入d_can_init函数
/*    {i2c2_init,    DEV_ON_BASEBOARD, PROFILE_NONE},*/ //删除i2c2的初始化函数
    {sgx_init,    DEV_ON_BASEBOARD, PROFILE_NONE},
   
    {NULL, 0, 0},
};

按照AM335X DCAN driver guide.pdf 对linux driver的CAN进行了配置,然后编译内核,将内核拷到SD卡中(我用的是SD启动),uboot和filesystem没有变,能正常启动,

问题:但是在/dev目录下找不到can0,can1的驱动,运行canconfig can0 start 提示Cannot find device "can0".查看串口显示记录,在启动过程中出现了boardname:A335BNLT board version : 000B,The board is a AM335x  Beaglebone Black..........等等,关于CAN的显示CAN device driver interface, CAN bus driver for Bosch D_CAN controller 1.0,can:controller area network core (rev 20090105 abi 8),can:raw protocol(rev 20090105),can:broadcast manager prorocol (20090105 t)。

PS:目前我只用了BBB,没有CAN扩展板,没有接CAN收发器,如果只看/dev目录下有没有驱动的话  CAN收发器应该可以不接,请教TI的大神帮我