This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSEVM6670L板上的GPIO



熟悉TMDSEVM6670L板的高手请指点一下,该板的技术资料说GPIO的引脚[0-13]被FPGA拿来用于Boot过程了,似乎[14-15]没有被拿来用做什么专门用途,而6670芯片本身的datasheet似乎说到14-15被兼用作PCIE的控制,那我们还能用这些GPIO口来做点事(比如实现一个10 Mbps的板间通讯)吗?

  • GPIO0~13是与boot pin复用管脚,所以在上电的过程这些管脚是用于控制boot mode,GPIO14~15是与PCIE mode复用管脚,在EVM上有把GPIO0~15通过80PIN expasion header扩展,所以也是可以与其他子卡进行GPIO通信。同时EVM也有SPI, UART, 及一些高速接口引出可用。