目前小弟手里有一块6467的评估板,我的开发环境是CCSV5,用的仿真器是SEED-XDS560V2,然后在开始建立工程的时候,我的编译出现了问题,然后我就进行修改,因为DM6467是一个ARM核和一个DSP核,我建立的是DSP的程序,因此在线调试的时候是在DSP核进行,将程序load进DSP核时候,CMD文件用的是TI官网6467的例程的那个LINKER的CMD,但是现在程序死在了tvp7002_setuo(mode),这句话,然后这里面死在了_I2C_tx_ready()这句话了。不知道是什么原因,希望得到帮助