This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
如何给6670EVM配置IP地址?
6670 的ethernet只能到MAC层,配置MAC地址,如果需要支持IP协议栈,需加载NDK
嗯,好的,谢谢,那怎么配置MAC的地址呢?
可以配置寄存器MACSRCADDR,调用csl函数CSL_CPSW_3GF_setPortMACAddress。
但是注意6670中设置的mac地址只是对流控起作用,对接收的包完全取决于ALE及PA等的配置。