您好:
请问在AM3359的NDK中,哪里提到了网口1和网口2的设置 ??
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,Jian Zhou:
我是CCS+sys/bios+NDK调试的,我是在SDK的adapter那个例程中,在CPSW+ICEv2上修改代码,然后在BB-Black中调试通网口1的MII模式,可以ping通,也可以正常通信。现在我照着BB-Black板子自己制作了一块板子,唯一不同的是将网口1换到网口2上,模式更改为RMII模式,PHY和AM3359的REF_CLK引脚为同时接上50MHz的有源晶振,代码部分我就是把pinmux修改为RMII复用和通信模式为RMII,别的地方没做改动,现在遇到的问题是,AM3359这边感觉NDK工作正常,可以正确读出网口2的MAC地址和我给它指定的IP地址,PHY这边我将其所有的寄存器值都读出来也都正确,包括模式,自动协商,PHY地址都没问题,而且在PC不断发ping指令的情况下测试了一下PHY的RX0引脚感觉得到的信号也是正常,但是去测试AM3359的TX引脚没有任何反应,不知道是什么原因,请给点排查的方法。谢谢了。
把网口改为RMII2,PHY是通的,但是TX没信号,是不是pinmux配的有问题啊