This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求助: C5515 指纹识别开发板 调试遇到问题 Error 0x80000242/-1143



开发环境:TMDXBDKFP5515 + CCS4,正确设置仿真器型号和处理器型号之后,debug就出现以下问题:

Error connecting to the target:
Error 0x80000242/-1143
Fatal Error during: Memory, Initialization, OCS,
The memory at 0x0000005F continually indicated it was 'not ready'
All memory operations currently in progress were aborted in order
to regain control of the processor.
This is considered a catastrophic event, but the debugger should
still be able to access memory and CPU registers.
System state has been altered.  It is strongly advised
that the processor should be reset before resuming execution,

求指点,谢谢!