This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

omapl137 nor flash引导问题



omapl137通过emifa接口cs2扩展nor flash,把boot引脚设置为nor flash引导时,发现不能从片上rom跳转到nor flash。 测量上电后emifa接口的cs2和oe信号,均为常高,没有读信号。 目前,处理器的上电顺序,先1.2v,间隔1ms多,3.3v。处理器未使用usb,未设计1.8v。 复位信号:晶振起振后,复位信号持续低电平290ms后变高。 请问电源和复位信号正常吗? 如果正常的话还有什么原因导致处理器不能正常引导?
  • #1. 连上仿真器看一下BOOTCFG寄存器,看boot mode设置是否正确。NOR boot的寄存器值应该为0x01.

    #2. 用的哪种NOR boot?读一下NOR flash的首地址的值是不是正确的配置字?

    #3. NOR flash的高位地址线的处理是否正确?应该接下拉电阻。