This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C5515连接仿真器问题

Other Parts Discussed in Thread: TMS320C5515

我之前使用的TI官方的DSP开发板EZDSP TMS320C5515,一直没问题,但是我将自己编写的USB程序转换成.BIN文件后下载在开发板外扩的NOFLASH后,现在一直不能与编译器(ccs4)连接了,提示的错误为C55xx: Error connecting to the target: Error 0x80000242/-1143 Fatal Error during: Memory, Initialization, OCS,  The memory at 0x0000005F continually indicated it was 'not ready' All memory operations currently in progress were aborted in order to regain control of the processor. This is considered a catastrophic event, but the debugger should  still be able to access memory and CPU registers. System state has been altered.  It is strongly advised that the processor should be reset before resuming execution, 请各位前辈多多指教,谢谢!

  • 可能是bin文件有问题,boot后的代码执行错误跑飞导致芯片状态异常而连不上仿真器。

    建议用镊子将flash的CS与V3.3短接,重新上电,这样板子就不会正常boot,就可以连接仿真器了。连上仿真器后将nor flash的内容擦掉就好了。

  • 谢谢,这样确实可以连接上仿真器了,但我有点疑问的是,我用的TI官方开发板的事例代码,其他事例代码都能正常从外部FLASH中运行,唯独这个USB的示例不行,我想请教这大概是哪方面的原因呢?另外我觉得即使BIN有问题,只是会程序不能实现应有的功能,怎么会影响仿真器呢?另外就是我也怀疑是CMD文件有误,但是我把其他能正常运行的程序中的CMD文件,替换到USB示例中,任然会出现之前那样的情况,敬请多多指教!

  • 你好,因为仿真器只是工具,真正的是CCS与芯片之间的相互通讯,仿真器就是这个相互通讯的桥梁。CCS是需要仿真器将芯片的一些状态反馈给它,只有是芯片的状态正确的情况下,才能正常调试。所以BIN有问题,有可能代码执行错误跑飞导致芯片状态异常,反馈给CCS的状态不正确,导致仿真器无法连接。

    看能否进行load symbol,加载烧写的out文件,单步跟一下,与仿真情况下对比一下芯片的状态有什么不同。