This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6657的SGMII测试

您好!

我使用的是C6657,CCS5.4 pdk_C6657_1_1_2_6。我的问题如下:

1.按照pdk_C6657_1_1_2_6测试,SGMII的Loopback测试不通。

2.pdk_C6657_1_1_2_6中的函数SGMII_config()中SGMII_REGS->RX_CFG,SGMII_REGS->TX_CFG,SGMII_REGS->AUX_CFG在所有的C6657相关的数据手册中根本就找不到。

3.pdk_C6657_1_1_2_6中的函数SGMII_config()中

if (config->loopbackEn) {
SGMII_REGS->CONTROL = 0x34;

}段落中,SGMII_REGS->CONTROL = 0x34;0x34不符合spruhh1.pdf,P189中关于CONTROL的说明。

谢谢!

Philip Den

2014-4-8