This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDXEVM6678LE新手入门问题



使用的是TMDXEVM6678LE仿真板,CCS5.2 使用Xds100v1,没有使用Xds560v2

1 仿真板型号问题
TMDSEVM6678L EVM Hardware Setup (use this link if you have a LE or LXE model),链接的是TMDXEVM6678L EVM Hardware Setup,TMDSEVM6678L和TMDXEVM6678L有什么关系吗?

2 TMDXEVM6678L EVM QUICK START GUIDE问题
厂商发送的CD中,EVM QUICK START GUIDE可以配置COM口的波特率为115200和查看IP address
(1)如何打开open HyperTerminal进行COM口配置
(2)如何打开HyperTerminal文本,查看IP地址

3 TMDXEVM6678LE改名了吗?
你好,我使用的是TI的EVM板TMDXEVM6678LE, 在网页中(processors.wiki.ti.com/.../MCSDK_VIDEO_2.0_Getting_Started_Guide)查看这个板子内容Supported Devices/Platforms,点击TMDXEVM6678LE时,跳出下面内容。是这块板子改名了吗?
The page you are looking for might have been removed, had its name changed, or is temporarily unavailable.
Please check the address bar to make sure the link is typed correctly, use the links below to locate the information you want, or search the site for another destination.


4 找不到hpdspua.c,如何解决

Can't find a source file at "/home/gtbldadm/ti/mcsdk_2_01_02_06/demos/hua/src/hpdspua.c"
Locate the file or edit the source lookup path to include its location.

5 CCS console and the UART端口
如何查看UART端口输出的信息
Note: The application will write messages simultaneously to the CCS console and the UART. Therefore you can use either the CCS Console or a serial port program to see them.


6 对TMDXEVM6678LE仿真板来说,使用XDS560V2XDS100V1有什么区别?

  • 1, TMDSEVM6678L和TMDXEVM6678L是一样的,TMDXEVM6678L是早期的版本;

    2,百度HyperTerminal;

    3, 你需要什么资料?

    4,你需要安装MCSDK,这个文件在C:\ti\mcsdk_2_01_02_06\demos\hua\src

    5,连接UART口到PC

    6,560是子卡,更快一些,XDS100集成在板上,速度较慢一点

  • 非常感谢您的回复。
    运行板子上的MCSDK HUA Demonstration,使用OOB自带程序或者mcsdk_2_01_02_06中的.out(目录C:\ti\mcsdk_2_01_02_06\demos\hua\evmc6678l),都无法正确给出Network Added: If-1,测试结果如下:

    The display(Network Added: If-1:)didn’t appeared.What to do for the problem?

    See the display below:

    QMSS successfully initialized

    CPPI successfully initialized

    PA successfully initialized

    HUA version 2.00.00.04

    Setting hostname to tidemo-PE9160

    MAC Address: 90-D7-EB-8C-CB-60

    Configuring DHCP client

    PASS successfully initialized

    Ethernet subsystem successfully initialized

    Ethernet eventId : 48 and vectId (Interrupt) : 7

    Registration of the EMAC Successful, waiting for link up ..

    Service Status: DHCPC    : Enabled  :          : 000

    Service Status: THTTP    : Enabled  :          : 000

    Service Status: DHCPC    : Enabled  : Running  : 000

    Service Status: DHCPC    : Enabled  : Fault    : 002

    Service Status: DHCPC    : Disabled :          : 000

    Service Status: DHCPC    : Enabled  :          : 000

  • TMDSEVM6678LE是自带仿真功能吗?不用配其它仿真器就能调试?