This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

我想问下AM335x系列wince 的 GPMC驱动问题



项目需要用wince写GPMC驱动和FPGA双口ram通信。我是参考linux的GPMC和FPGA通信驱动编写。我在linu,示波器x下测试双口ram能正常工作。

代码如下,但是很多可能有错或理解不清,只能读写gpmc的寄存器,但是无法读写FPGA的ram数据,示波器也没信号

 在bsp_padcfg.h中添加

#define FPGA_PADS \  

PAD_ENTRY(GPMC_AD0,         MODE(0) | AM335X_PIN_INPUT_PULLUP)         \

PAD_ENTRY(GPMC_AD1,         MODE(0) | AM335X_PIN_INPUT_PULLUP)       /* NOR_AD1 */   \

 PAD_ENTRY(GPMC_AD2,         MODE(0) | AM335X_PIN_INPUT_PULLUP)       /* NOR_AD2 */   \  

PAD_ENTRY(GPMC_AD3,         MODE(0) | AM335X_PIN_INPUT_PULLUP)       /* NOR_AD3 */   \  

PAD_ENTRY(GPMC_AD4,         MODE(0) | AM335X_PIN_INPUT_PULLUP)       /* NOR_AD4 */   \  

PAD_ENTRY(GPMC_AD5,         MODE(0) | AM335X_PIN_INPUT_PULLUP)       /* NOR_AD5 */   \

 PAD_ENTRY(GPMC_AD6,         MODE(0) | AM335X_PIN_INPUT_PULLUP)       /* NOR_AD6 */   \  

PAD_ENTRY(GPMC_AD7,         MODE(0) | AM335X_PIN_INPUT_PULLUP)       /* NOR_AD7 */   \  

PAD_ENTRY(GPMC_AD8,         MODE(0) | AM335X_PIN_INPUT_PULLUP)       /* NOR_AD8 */   \  

PAD_ENTRY(GPMC_AD9,         MODE(0) | AM335X_PIN_INPUT_PULLUP)       /* NOR_AD9 */   \  

PAD_ENTRY(GPMC_AD10,        MODE(0) | AM335X_PIN_INPUT_PULLUP)       /* NOR_AD10 */  \  

PAD_ENTRY(GPMC_AD11,        MODE(0) | AM335X_PIN_INPUT_PULLUP)       /* NOR_AD11 */  \

 PAD_ENTRY(GPMC_AD12,        MODE(0) | AM335X_PIN_INPUT_PULLUP)       /* NOR_AD12 */  \

 PAD_ENTRY(GPMC_AD13,        MODE(0) | AM335X_PIN_INPUT_PULLUP)       /* NOR_AD13 */  \  

PAD_ENTRY(GPMC_AD14,        MODE(0) | AM335X_PIN_INPUT_PULLUP)       /* NOR_AD14 */  \  

PAD_ENTRY(GPMC_AD15,        MODE(0) | AM335X_PIN_INPUT_PULLUP)       /* NOR_AD15 */  \  

PAD_ENTRY(GPMC_A0,          MODE(0) | AM33XX_PIN_OUTPUT | AM33XX_PULL_DISA)          /* NOR_AD0 */   \  

PAD_ENTRY(GPMC_A1,          MODE(0) | AM33XX_PIN_OUTPUT | AM33XX_PULL_DISA)          /* NOR_AD1 */   \

 PAD_ENTRY(GPMC_A2,          MODE(0) | AM33XX_PIN_OUTPUT | AM33XX_PULL_DISA)          /* NOR_AD2 */   \  

PAD_ENTRY(GPMC_A3,          MODE(0) | AM33XX_PIN_OUTPUT | AM33XX_PULL_DISA)          /* NOR_AD3 */   \  

PAD_ENTRY(GPMC_A4,          MODE(0) | AM33XX_PIN_OUTPUT | AM33XX_PULL_DISA)          /* NOR_AD4 */   \  

PAD_ENTRY(GPMC_A5,          MODE(0) | AM33XX_PIN_OUTPUT | AM33XX_PULL_DISA)          /* NOR_AD5 */   \  

PAD_ENTRY(GPMC_A6,          MODE(0) | AM33XX_PIN_OUTPUT | AM33XX_PULL_DISA)          /* NOR_AD6 */   \  

PAD_ENTRY(GPMC_A7,          MODE(0) | AM33XX_PIN_OUTPUT | AM33XX_PULL_DISA)          /* NOR_AD7 */   \  

PAD_ENTRY(GPMC_A8,          MODE(0) | AM33XX_PIN_OUTPUT | AM33XX_PULL_DISA)          /* NOR_AD8 */   \  

PAD_ENTRY(GPMC_A9,          MODE(0) | AM33XX_PIN_OUTPUT | AM33XX_PULL_DISA)          /* NOR_AD9 */   \

 PAD_ENTRY(GPMC_A10,         MODE(0) | AM33XX_PIN_OUTPUT | AM33XX_PULL_DISA)             /* NOR_AD10 */  \

 PAD_ENTRY(GPMC_A11,         MODE(0) | AM33XX_PIN_OUTPUT | AM33XX_PULL_DISA)             /* NOR_AD11 */  \  

PAD_ENTRY(GPMC_ADVN_ALE,    MODE(0) | AM33XX_PULL_DISA)        /* NAND_ADV_ALE */ \  

PAD_ENTRY(GPMC_OEN_REN,     MODE(0) | AM33XX_PULL_DISA)         /* NAND_OE */ \  

PAD_ENTRY(GPMC_WEN,         MODE(0) | AM33XX_PULL_DISA)        /* NAND_WEN */  \

 PAD_ENTRY(GPMC_BE0N_CLE,    MODE(0) | AM33XX_PULL_DISA)        /* NAND_BE_CLE */  \  

PAD_ENTRY(GPMC_CSN1,        MODE(0) | AM33XX_PULL_DISA)        /* MMC1_CLK */  \  

PAD_ENTRY(GPMC_CLK,         MODE(0) | AM33XX_PULL_DISA)  

 

 

在bsp_padcfg.c中添加

 

{ FPGAPads,    AM_DEVICE_FPGA,          PROFILE_3,                                    DEV_ON_DGHTR_BRD},   

 

最后编写驱动fpga.c

 

#define STNOR_GPMC_CONFIG1 0x28601000     // no wait, 16 bit, non multiplexed

#define STNOR_GPMC_CONFIG2 0x00011001

 #define STNOR_GPMC_CONFIG3 0x00020201   // we don't use ADV

 #define STNOR_GPMC_CONFIG4 0x08031003 

 #define STNOR_GPMC_CONFIG5 0x000f1111

#define STNOR_GPMC_CONFIG6 0x0f030080

#define BSP_GPMC_PSOC_CONFIG7      0x00000F41         // Base address 0x1000000, 16MB window

#define BSP_GPMC_PSOC_CONFIG7_1    0x00000F01     

 

DWORD FGA_Init(LPCTSTR szContext, LPCVOID pBusContext)

 {

DWORD rc = (DWORD)NULL;

 NKDbgPrintfW(TEXT("FPGA init.\n"));

 PHYSICAL_ADDRESS pa;

 InitializeCriticalSection(&g_csOpen);   

InitializeCriticalSection(&g_csRead); 

 InitializeCriticalSection(&g_csWrite); 

 FpgaDevice *pDevice = NULL;  

pDevice = (FpgaDevice *)LocalAlloc(LPTR, sizeof(FpgaDevice));  

if (pDevice == NULL) {   

NKDbgPrintfW(TEXT("FPGA init error.\n"));  

 return -1;  }

 int error;  

UINT32 val;

  UINT32 vison;

 pa.QuadPart =  GPMC_BASE_ADDR; 

 // AM3XX_GPMC_REGS_PA is defined as 0x50000000

 pDevice->pGpmc = (AM3XX_GPMC_REGS *)MmMapIoSpace(pa, sizeof(AM3XX_GPMC_REGS), FALSE);

 DEBUGMSG(ZONE_ERROR,(L"pGpmc_base= %x\n", pDevice->pGpmc));  

vison=INREG32(&pDevice->pGpmc->GPMC_REVISION);    

 DEBUGMSG(ZONE_ERROR,(L"vison = %d.%d\n",(vison >> 4) & 0x0f, vison & 0x0f));  

OUTREG32(&pDevice->pGpmc->GPMC_CONFIG, BSP_GPMC_PSOC_CONFIG7_1); // disabling the chip select  

DEBUGMSG(ZONE_ERROR,(L"gpmc base = %x\n",pDevice->pGpmc));

 OUTREG32(&pDevice->pGpmc->GPMC_CONFIG, (INREG32(&pDevice->pGpmc->GPMC_CONFIG))|0x00000002); //setting LIMITEDADDRESS to 1.  

val =INREG32(&pDevice->pGpmc->CS[1].GPMC_CONFIG7);

 DEBUGMSG(ZONE_ERROR,(L"GPMC_CS_CONFIG7 value default 0x%x\n", val));  

OUTREG32(&pDevice->pGpmc->CS[1].GPMC_CONFIG1, STNOR_GPMC_CONFIG1);

 OUTREG32(&pDevice->pGpmc->CS[1].GPMC_CONFIG2, STNOR_GPMC_CONFIG2);  

OUTREG32(&pDevice->pGpmc->CS[1].GPMC_CONFIG3, STNOR_GPMC_CONFIG3);

 OUTREG32(&pDevice->pGpmc->CS[1].GPMC_CONFIG4, STNOR_GPMC_CONFIG4);  

OUTREG32(&pDevice->pGpmc->CS[1].GPMC_CONFIG5, STNOR_GPMC_CONFIG5);

 OUTREG32(&pDevice->pGpmc->CS[1].GPMC_CONFIG6, STNOR_GPMC_CONFIG6);  

OUTREG32(&pDevice->pGpmc->CS[1].GPMC_CONFIG7, BSP_GPMC_PSOC_CONFIG7);

 val =INREG32(&pDevice->pGpmc->CS[1].GPMC_CONFIG7);

  DEBUGMSG(ZONE_ERROR,(L"GPMC_CS_CONFIG7 value 0x%x\n", val));

  pa.QuadPart = 0x1000000;

 pDevice->fpga_base = (volatile FPGAREG16 *)MmMapIoSpace(pa, 2048, FALSE);  

DEBUGMSG(ZONE_ERROR,(L"fpga_base= %x\n", pDevice->fpga_base));

rc = (DWORD)pDevice;  

return rc;

 

DWORD FGA_Read(DWORD context, VOID *pBuffer, DWORD size)

 {  int status = 0,i,tmp;

 RETAILMSG(ZONE_ERROR,(L"read here"));

 int len; // UCHAR* pData = (UCHAR*)pBuffer;

  FpgaDevice *pDevice =(FpgaDevice *)context;  //EnterCriticalSection(&g_csRead);  // VALIDATE_ADDR_PORT(basead)  

DEBUGMSG(ZONE_ERROR,(L"fpga base = %x\n",pDevice->fpga_base));

 len=size;  for(i=0;i<len;i=i+2)  

{  

 tmp = INREG16(&pDevice->fpga_base+i);  

 pDevice->userbuff[i] = tmp&0xff;   pDevice->userbuff[i+1] = (tmp>>8)&0xff;   

 } 

 //  DEBUGMSG(ZONE_ERROR,(L"read = %x%x\n",pBuffer[0],pBuffer[1]));

 memcpy(pBuffer,pDevice->userbuff,size);

// LeaveCriticalSection(&g_csRead);  

return size;  

}

 

我想知道应该如何写,找不到参考资料