OMAPL138 的MMC/SD接口能够支持SDXC卡吗?能够支持SD卡最大容量是多少?(环境:在LINUX操作系统下,内核版本为2.6.33)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
OMAPL138 的MMC/SD接口能够支持SDXC卡吗?能够支持SD卡最大容量是多少?(环境:在LINUX操作系统下,内核版本为2.6.33)
你好,OMAPL138 的MMC/SD接口不支持SDXC卡,请看下面特性说明:
The MMC/SD card controller supports the following industry standards (with the exception noted below):
• MMC (Multimedia Card) Specification v4.0
• SD (Secure Digital) Physical Layer Specification v1.1
• SDIO (Secure Digital Input Output) Specification v2.0
您好,首先非常感谢您的回答,在我发了这封求助帖之后,我买了一张SDXC的卡(64GB),进行了实际的测试(环境:OMAPL138 Linux kernel 2.6.33),结果如下:
......................................................................................................................................
mmc0: new high speed SDHC card at address 0007
mmcblk0: mmc0:0007 SD64G 59.0 GiB
mmcblk0: p1
eth0: attached PHY driver [Generic PHY] (mii_bus:phy_addr=1:00, id=221613)
IP-Config: Guessing netmask 255.255.255.0
IP-Config: Complete:
device=eth0, addr=192.168.1.3, mask=255.255.255.0, gw=255.255.255.255,
host=192.168.1.3, domain=, nis-domain=(none),
bootserver=255.255.255.255, rootserver=192.168.1.112, rootpath=
...................................................................................................................................
可以看出卡被识别了,但是别成的却是SDHC,并且我在开发板 linux 环境下进行了对卡进行了读写测试,能够正常读写,然后我也查看了相应工业标准的相应信息,结果诚如您所说支持的为SDHC。所以现在感到非常困惑,我想知道为什么会产生这种现象,在这种情况下还能否正常使用?期待着您的答复,不胜感激!