This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

6678EVM boot的问题

专家好,最近在学习6678EVM的boot,遇到了点问题。我的步骤是这样的:

拨码开关置于No boot模式,首先烧写I2C以及配置IBL,console显示烧写成功。然后烧写一个点灯程序的.bin文件(CCS工程运行是没有问题的)到NAND flash,console也显示烧写成功。然后将研华官网下载到的开发板上FPGA的源代码(稍微做了修改,只加了一个分频产生1Hz的输出信号)生成的.bit文件重新下载到FPGA中,灯是能够闪烁起来的,但是问题是当我断电后,把拨码开关设置成I2C POST boot模式(IBL NAND boot on image 0???这里我不太清楚拨码开关要怎么设置)后重新上电,发现灯并没有闪烁,而此时当我重新再下载一次FPGA的源码生成的.bit文件到FPGA中后发现灯是闪烁的。我不太明白这是个什么状况,所以想请问一下,可能是什么原因导致了这种情况。感谢您们的帮助,不胜感激!

x 出现错误。请重试或与管理员联系。