Other Parts Discussed in Thread: 66AK2E05
各位专家及大牛,我在调试C6678的千兆网时,使用了CCS自带的MCSDK下的hua daemo例程,在其中网络连接建立后加入了自己用SOCKET向计算机(xp系统)发送数据的函数,实际测试中发现采用IPPROTO_UDP协议时,发送速率能达到400Mbps左右,发送200万个包其中大概有4、5个丢失,请问用socket传输速率(最好是你们实际中实现的速率)最大能达到多少?我后来想改成IPPROTO_TCP(参照的是NDK目录下spru523文档中的例子),但用connect函数建立连接时始终失败,错误代码61,我查了一下是拒绝连接,请问这个是什么原因及怎么解决。
另外,我看了一下PA_EmacExample那个例子,这个例子对网络的配置是不是比hua daemo更底层?在zhen kong发表的帖子“C6678千兆网调试”中Marvin Liang 回复说“例子中注释掉 CSL_SGMII_enableLoopback (macPortNum); cpsw_mng.c 即可取消internal loopback模式,请参看附件中的代码在C6678 EVM上来实现千兆以太网的SGMII和SERDES的配置。”我照着做了PLL能锁定,但程序中有一段查询SGMII状态寄存器的代码,显示始终无连接(寄存器连接状态位一直为0,网线已经连接好),程序在这死循环不能继续运行,请问是否需要配置MDIO?如果需要怎么配置?例子中有一个Init_Mdio的函数,但没有实现。如果不需要配置,那怎么才能建立连接?
谢谢!