This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6678开发板预留的接口能否和FPGA的SRIO连接?



TMS320C6678这个开发板有很多接口,我现在自己画了一个赛灵思K7系列FPGA的单板,想和TMS320C6678连接,我看其他资料显示需要用4个SRIO连接,不知道TMS320C6678是否预留了4个高速SRIO接口连接器?能否通过外开发板已有的连接器和FPGA的高速SRIO联通

  • 6678的EVM板上SRIO4个Lane都引出到AMC接口上,你可以从6678 EVM 的原理图上看到,如果你要和你的fpga对接,你可以考虑使用AMC插槽的方式,这4个SRIO Lane是独立的,每一个最大可以提供5Gbps的线速率,总共是20Gbps,你可以根据自己的需要来决定使用几个

  • FEMALE HEADER 2x40P 1.27mm 180D(F) SMD 22L8742

    这个的80针的连接器资料有没有,我想画电路板可是BOM表上就给出了上述信息,我去百度GOOGLE都没查到该连接器....让我怎么画电路板呀....