This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAPL138锁相环配置问题,处理器时钟太高仿真器断开连接



     用了OMAPL138这块片进行SOC开发的时候,当我把ARM的时钟调到超过200M时,仿真器就会断开连接,但是程序依然在跑并且执行正确

     我用的合众达公司的SEED XDS560 PLUS仿真器,仿真器软件版本号是V2.6,开发环境是CCS5.5,外部时钟源是24M,精度30ppm,负载电容为22p的无源石英晶体谐振器

    请问可能的问题是什么

  软件报出的故障如下:

ARM9_0: Error: (Error -1029 @ 0x2B5F) Invalid data read from ICECrusher register. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 5.1.232.0)
ARM9_0: Unable to determine target status after 20 attempts
ARM9_0: Failed to remove the debug state from the target before disconnecting. There may still be breakpoint op-codes embedded in program memory. It is recommended that you reset the emulator before you connect and reload your program before you continue debuggin