请问,假如我用dm365作视频编解码,先采集720*576的视频,然后在LCD上以320*240输出,我该如何修改或添加代码来使用resizer模块?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请问,假如我用dm365作视频编解码,先采集720*576的视频,然后在LCD上以320*240输出,我该如何修改或添加代码来使用resizer模块?
在SDK中DMAI文件夹下有例子,可以参照该目录下video_loopback_resizer的例程
我试过,会出现以下错误:
davinci_resizer davinci_resizer.2:
mode doesn't allow multiple instances
encode: linux/dm365/Resize.c:293: Resize_execute: Assertion `hResize' failed.
Aborted
是不是该修改resize.c文件?
这个错误的提示resizer句柄被重复打开,请问你是否已经在运行其他程序(可能会用到resizer的),然后跑的这个demo。最好直接跑demo,结合源码来理解如何使用resizer
你好,我是用dvsdk包里的encode程序加以修改,使之输出到LCD上,好像不大可能同时使用了两个resizer,而且它应该支持两路resizer的吧?