This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6678: 关于C6678 SRIO提供例程问题

Part Number: TMS320C6678

我现在阅读提供的demo  device_srio_loopback.c 文件,函数 SrioDevice_init中代码,手册中寄存器是只读属性,为什么可以写入,手册中寄存器只有11个选项,但是代码为什么有14个输入,有的选项我没有找到

    /* TODO: Configure the processing element features
     *  The SRIO RL file is missing the Re-transmit Suppression Support (Bit6) field definition */
    peFeatures.isBridge                          = 0;
    peFeatures.isEndpoint                        = 0;
    peFeatures.isProcessor                       = 1;
    peFeatures.isSwitch                          = 0;
    peFeatures.isMultiport                       = 0;
    peFeatures.isFlowArbiterationSupported       = 0;
    peFeatures.isMulticastSupported              = 0;
    peFeatures.isExtendedRouteConfigSupported    = 0;
    peFeatures.isStandardRouteConfigSupported    = 1;
    peFeatures.isFlowControlSupported            = 1;
    peFeatures.isCRFSupported                    = 0;
    peFeatures.isCTLSSupported                   = 1;
    peFeatures.isExtendedFeaturePtrValid         = 1;
    peFeatures.numAddressBitSupported            = 1;
    CSL_SRIO_SetProcessingElementFeatures (hSrio, &peFeatures);
CSL_IDEF_INLINE void CSL_SRIO_SetProcessingElementFeatures
(
CSL_SrioHandle hSrio,
SRIO_PE_FEATURES* ptrPEFeatures
)
{
Uint32 value = 0;

/* Initialize the various fields in the register */
CSL_FINS (value, SRIO_RIO_PE_FEAT_BRDG, ptrPEFeatures->isBridge);
CSL_FINS (value, SRIO_RIO_PE_FEAT_MEM, ptrPEFeatures->isEndpoint);
CSL_FINS (value, SRIO_RIO_PE_FEAT_PROC, ptrPEFeatures->isProcessor);
CSL_FINS (value, SRIO_RIO_PE_FEAT_SW, ptrPEFeatures->isSwitch);
CSL_FINS (value, SRIO_RIO_PE_FEAT_MULT_P, ptrPEFeatures->isMultiport);
CSL_FINS (value, SRIO_RIO_PE_FEAT_FLOW_ARB, ptrPEFeatures->isFlowArbiterationSupported);
CSL_FINS (value, SRIO_RIO_PE_FEAT_MC, ptrPEFeatures->isMulticastSupported);
CSL_FINS (value, SRIO_RIO_PE_FEAT_ERTC, ptrPEFeatures->isExtendedRouteConfigSupported);
CSL_FINS (value, SRIO_RIO_PE_FEAT_SRTC, ptrPEFeatures->isStandardRouteConfigSupported);
CSL_FINS (value, SRIO_RIO_PE_FEAT_FLOW_CTRL,ptrPEFeatures->isFlowControlSupported);
CSL_FINS (value, SRIO_RIO_PE_FEAT_CRF, ptrPEFeatures->isCRFSupported);
CSL_FINS (value, SRIO_RIO_PE_FEAT_CTLS, ptrPEFeatures->isCTLSSupported);
CSL_FINS (value, SRIO_RIO_PE_FEAT_EXT_FEA, ptrPEFeatures->isExtendedFeaturePtrValid);
CSL_FINS (value, SRIO_RIO_PE_FEAT_EXT_AS, ptrPEFeatures->numAddressBitSupported);

hSrio->RIO_PE_FEAT = value;
}